This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq77pl900的3号和4号管脚短路,并且芯片发热?



请教专家,使用20伏电源供电,使用10个180欧姆电阻串联模拟电池,这时PL900芯片不发热,电流正常。此时使用200欧姆短接PACK+和BAT+,把PL900唤醒时,电流达到0.45安培,芯片会发热,并且REG1和REG2不会出现3.3和5V电压。

之后测量3号和4号管脚时,发现两个引脚间短路,并且REG1和REG2不会出现3.3和5V电压

补充一下,按照开发板的手册画的电路图,焊接的,原件的型号也是按照手册做的。只是连接电池的时候,没有问题,当从唤醒时才会出现上述问题,并且一旦发生上述问题,芯片3号和4号管脚,就会短路,并且不会恢复,