Other Parts Discussed in Thread: LM5010
LM5010使用情况:
1.LM5010作为48V转15V,后续有15V转5V芯片;启动后,5V电压为0.3A
2.当5V负载突然增大时,5V的负载大概为0.5A,此时15V被拉低到5V电压.
这个问题是如何产生的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
单独测15V以及5V的带载能力。
你需要注意2个转换中,功率电感饱和电流足够。
其次影响带载能力还和芯片的layout有关,功率回路尽量小, 以及注意sense电路。(datasheet有参考)