选用了TPS62745作为转压芯片,根据文档输入电压范围是3.3--10V,但是买的9V方块电池 全新的时候有10.8V左右,不知道能不能使用?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不推荐使用,TPS62745输入耐压12V,所以使用10.8V左右,芯片不会损坏。
但是芯片的在规格书的详细规格比如精度,漏电流等参数都是在3.3V-10V的输入电压范围内测量的,超出范围,无法保证芯片规格书参数规定的规格。
多谢,那有没有推荐的芯片?当初选择TPS62745这一款的原因是电压合适,功耗极低(0.4uA)。 没想到新电池的电压会这么高。
Hi
超过10v都有过压风险,不建议使用。
或者建议你搞用其他型号电池,例如存在并联,使得输入电压稍微低一些。
或者说你能接受的最大静态电流时多大? 超过10V以上输入,看了一下,静态电流都相对大一些了。
另外你的电流需求最大是多少?
你好,静态电流最好是5uA以下的吧。系统是接NBIOT的,所以平时都是在uA级别工作的,只有发射的时候电流大些,要保证300mA的工作电流。
Hi
推荐TPS62175(如果是固定3.3V输出,可以选择TPS62177)