1,没有电池时,适配器接入,LED等闪烁,这应该是正常的。
2,当7.7V的电池插上,适配器接入时,LED却是灭的。AVCC这个引脚电压8.2和7.7之间跳变?VREF的电压也在跳变。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1,没有电池时,适配器接入,LED等闪烁,这应该是正常的。
2,当7.7V的电池插上,适配器接入时,LED却是灭的。AVCC这个引脚电压8.2和7.7之间跳变?VREF的电压也在跳变。
Hi
这是个降压转换的充电芯片,如果电池是7.7V, AVCC这个引脚电压8.2和7.7之间跳变, 那么输入电压是多少? 也是在跳变吗(范围)?
测试一下OVPSET的电压是多少?(是否也在跳变?)
应该是过流了。换了稳压源,设定12V/2.5A。LED等会常亮,但是稳压源的输出电流达到2.5A。AC采样电阻R1004两端的电压50mV。R1008两端量不到电压??后端负载已经断开了。R1020断开了
Hi
断电测试SW脚是否与GND短路或者低阻抗,有可能芯片已经烧掉了。