This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于电源热切换 与 理想二极管



情况是这样:

便携设备,有两个电源: 1.5V AA单节电池,3.7V锂电池。 电流最大2A。

两个电源通过DCDC升压到9-12V。 现在需要两个理想二极管,把1.5V和3.7V隔离开, 可不可以用两个 PMOS 代替二极管,把 D S极反过来,就像防反接电路一样呢

LT4352之类的器件倒是可以达到要求,但是其静态消耗电流mA级别,对单节电池供电不合适。