This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6657用的UCD9222+7242这套电源方案,板子正常工作电压只在6.8V到8.1V之间

Other Parts Discussed in Thread: UCD9222, UCD7242

自己做的6657的板子,电源用的9222+7242这套方案,参考官板画的,目前板子只在6.8V到8.1V之间正常工作,

目前发现板子画的有几处问题:

    1,UCD9222那里反馈的EAP/EAN两组信号没有画成差分线,也没放在dsp附近;
    2,UCD7242输出那里电容大小和官板不一样,

目前希望电源能在12V或5V上工作,但5V和12V,dsp均不能启动,电源提供5V时UCD7242没有输出,12V输出电压正常,但DSP不能正常工作,

有位TI工程师说:对于DSP来说,只要能正确的提供供电电压和上电时序,正确的时钟输入和RESET信号,就能跑起来。

那么UCD7242可能那个地方会影响到输出电压呢?