我现在用BQ2000给24V镍氢电池充电,就是按照2000的评估板原理图和做的板,输入32V,大约最大0.65A左右充电,
当我把充电最高电压设置的是28.2V左右时,0.6A充电到28.2时电流开始缓慢下降,最后停止充电。
但是当我把电压设置的稍高点也就是28.6V左右时,充电电压到28.6V时,电流不会一直下降,下降到0.18A左右时就一直充,都这样几个小时了也不关断,我想用万用表量下4脚电压,表笔一接触上去就关断不充电了,电压1.95V多快2V了。一不接触就又恢复充电,电流0.18A左右,请问这是怎么回事啊??