请问TPS54331DDAR Eco-mode 轻载高效模式能关闭吗?或有对应不带这个功能的IC推荐吗?
问题描述:
我使用TP54331 DC-DC降压电路
输入:6.4V电池供电
输出:3.9V
当电池电压下降到5V以下时,系统进入睡眠模式,电流为微安级,此时TP54331进入了Eco 模式,输出不正常,才2伏多还一直跳动。系统电流增大到100mA输出恢复正常。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Eco-mode不能关闭,你的问题和Eco-mode应该没有关系。
你的原因应该是输入电压过低,芯片内部被最小关断时间限制,所以才会出现输出电压不稳的问题。
建议你用示波器看下波形,不要用万用表,这样便于问题的定位
对于进入Eco-mode,主要看电流是否低于 160 mA (typical),然后Comp脚电压才会被锁在0.5V
When the peak inductor current is lower than 160 mA (typical), the COMP pin voltage falls to 0.5 V (typical) and the device enters Eco-mode. When the device is in Eco-mode, the COMP pin voltage is clamped at 0.5-V internally which prevents the high-side integrated MOSFET from switching.
Comp电压是被锁在0.5V,不是低于0.5V。
另外你看下boot电容两端的电压有没有小于2.1V, 如果是的,那问题就是压差过小导致