This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH05050WAH低温问题



你好,我用的两个PTH05050WAH给DSP供电,5V输入,两个模块分别输出3.3V和1.2V,每个PTH05050WAH的输入端都接了100uF的电容TPME107K020R0035,输出端也同样接了100uF的电容TPME107K020R0035,常温工作时没有问题,但温度降到-30℃到-40℃时电源输出就变得不稳定,DSP会出现无法启动或者自动复位的情况,我的5V电源是单独的一块电源板,转换模块用的是THL 3-2411WI,电源板通过双排插针转接2次后接到PTH05050WAH和DSP的这块板,5V传输的长度大概有15厘米,请问有没有可能是5V传输线太长或者双排插针有问题,还是我给PTH05050WAH选的电容不合理,多谢!

  • 模块的最低工作电压可以达到-40度,检查一下电容的datasheet,看一下最低温度是多少度,或者更换电容测试

  • 请问该问题有突破吗?
  • Hi
    datasheet上有说明,低于0°C是不建议用电解电容的。在低温下,容值是有跌落。
    For most applications, a high quality computer-grade aluminum electrolytic capacitor is adequate. These capacitors provide decoupling over the frequency range, 2 kHz to 150 kHz, and are suitable for ambient temperatures above 0°C. For operation below 0°C tantalum,
    ceramic or OS-CON type capacitors are recommended. When using one or more non-ceramic capacitors, the calculated equivalent ESR should be no lower than 4 mΩ (7 mΩ using the manufacturer's maximum ESR for a single capacitor).
  • 你好,我用了钽电容以及os-con的铝聚合物电容,但是低温时THL 3-2411WI输出的5V确实不如常温,现在想能否在PTH05050WAH输出后再加一级LDO稳压输出,请问LDO对纹波噪声的抑制效果如何,我用的DSP型号是TMS320C6713BGDP-A200,请问3.3V和1.2V各需要多大的电流,TI是否有对应的LDO推荐?多谢!
  • THL 3-2411WI输入电压是24V,温箱测试时是由外部的24V电源通过1米多长的电源线引入到温箱里接到THL 3-2411WI的输入端,请问这1米多长的电源线是否可能有影响呢?
  • Hi
        低温异常多与容值跌落有关。 有导线,一般异常为寄生电感偏大,在电源输入产生spike,甚至过压。此时可以在导线接入处增加一个较大的电容。

  • 您说的对,低温测试是用继电器来控制电源的通断,继电器的存在会导致产生spike吗,比较奇怪的是常温和高温都工作正常,只有低温时出问题,在导线接入处加电容我也试过了,用单个型号为A759MX447M1HAAE028的铝聚合物电容,效果不好,用两个A767MU107M1HLAE027铝聚合物电容并联有一定效果,所以是不是在加大电容的前提下同时还要尽量降低电容的ESR值,这样效果才好呢?多谢!

  • 还想请问一下,由于低温测试时继电器工作频率较高,大约2分钟通断一次,如果每次都产生spike,如此频繁的脉冲电压,会影响电容的性能吗?因为现在看实验现象都是工作一段时间后才出问题,多谢!