This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这两天,拿另一块板卡【板卡2】测试,测试过程中,也出现类似的现象,现描述入下:
1.初步调试,9-32V输入变化调整,20V输出正常。但,接近20V输入时,输入电流过大。
2.输入电压在17.45V-23.75V范围内时,输入电流急剧增大,最大到可达到1A左右。检测SW1和SW2波形大致如下图所示:(但在区间9-17V,24-32V,SW1,SW2波形正常,输入电流约0.09A左右)
3. 原输入9-32V,VCC输出正常,约7.35V左右。后焊接续流二极管(注:续流二极管都用的B550C-13-F)如下图所示,测试时发现VCC输出只有4.5V左右。
4.卸去续流二极管后,测量VCC仍然为4.5V。该情况空载输出20V,输入15V@0.166A情况下,测量SW1,SW2波形如下图。(通道1为SW1,通道2位SW2,空载输出20V)
【板卡2】更换芯片后,现象与1.和2.相同。即:
1.初步调试,9-32V输入变化调整,20V输出正常。但,接近20V输入时,输入电流过大。
2.输入电压在17.45V-23.75V范围内时,输入电流急剧增大,最大到可达到1A左右。检测SW1和SW2波形大致如下图所示:(但在区间9-17V,24-32V,SW1,SW2波形正常,输入电流约0.09A左右)
后增加1个100uF输出电容,对应输入电流急剧增大的输入电压范围减小,大概18V-23V.
再增加1个100uF输出电容,对应输入电流急剧增大的输入电压范围进一步减小,大概21V-22V.
随后,卸除以上2*100uF电容,焊接1个470uF输出电容,Vout空载输出不正常。卸除470uF输出电容后,Vout正常输出20V,但测量VCC又只有4.13V左右;对应现象和4.相同,即:
4.空载输出20V,输入15V@0.166A情况下,测量SW1,SW2波形如下图。(通道1为SW1,通道2位SW2)
【板卡2】再次更换芯片后,①将ISNS(-) ISNS(+)管脚Short,②调整如下图电容值到220pF,问题基本得到解决。
初步调试,9-32V输入变化调整,20V输出正常;buck,boost,buck-boost,SW1,SW2波形都正常;VCC输出正常。输入电压在9V增加至32V的过程中,输入电流逐渐减小。但在输入电压从14V调整至9V的过程中,20V空载输出时,输入电流由98mA左右逐渐增加至156mA左右。100mA输入电流好像稍微有点大。
****************************************************************************************************************************************************************************
根据【板卡2】对【板卡1】做样同样修改,如该帖标题描述问题,【板卡1】空载输出20V正常,但VCC输出仍然只有3.3V左右,非常奇怪。(VCC实际输出3.4V的样子,已经大于3.3V了,根据datasheet 8.4.1,LM5175已经Operating, Switching enabled)但不知道是什么原因导致VCC只输出那么小的电压?理论VCC应该输出7.35V才是。