This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24113和BQ24103中,CMODE 和TTC相关问题。

Other Parts Discussed in Thread: BQ24133

1.TTC是用于控制充电时间的,但是有一些细节上的东西看的不是很明白:比如我们设置TTC充电0~100的时间为三小时,那么假设我们从百分之五十的电开始冲,那么一个半小时后电池充满时充电芯片的反应逻辑是怎么样的?TTC脚反应逻辑是怎样的?

2.CMODE和TTC在细分场景下的应用孰优孰劣?各自有哪些优势呢?现在纠结于器件选型。

datasheet没有看的很明白,希望大神解释一下,谢谢!

  • Hi,

    TTC 用于设置快速充电安全定时器。
    可以参考bq24133 数据手册第五页 www.ti.com/.../getliterature.tsp
    Safety Timer and termination control. Connect a capacitor from this node to AGND to set the fast charge safety timer(5.6 min/nF). Precharge timer is internally fixed to 30 minutes. Pull the TTC to LOW to disable the charge termination and safety timer. Pull the TTC to HIGH to disable the safety timer but allow the charge termination.

    1.比如我们设置TTC充电0~100的时间为三小时,那么假设我们从百分之五十的电开始冲,那么一个半小时后电池充满时充电芯片的反应逻辑是怎么样的?TTC脚反应逻辑是怎样的?

    在一个半小时电池充电的过程包括CC、CV模式,最终充电完成,电流截止。由于设置TTC为三小时快充时间,该定时器并未溢出,TTC不会动作。

    2.CMODE是用于切换Pre-charge与Fast-charge模式的host control 引脚。当CMODE为低时,通过ISET2配置pre-charge与termination current;当CMODE为高时,通过ISET1配置Fast-charge current.
    CMODE与TTC是两个不同的功能,请参考数据手册www.ti.com/.../bq24103.pdf