This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2841带动态负载,输出不稳定,为什么?

Other Parts Discussed in Thread: LM2841

LM2841输入电压24V,输出5V,电路:

空载时负载在5mA左右,但是需要周期性(大约2秒左右)点亮LED,LED输出20mA左右,发现只有一点亮LED,

输出电压被拉低100mA,LED关闭,输出电压回升,这是为何?

空载时SW波形:

LED点亮,输出20mA,SW波形: