This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ25700A 对于不知名适配器的电流优化器ICO



你好,对于不知名适配器的电流优化器ICO,例如我设置的输入电流是2A,但是适配器实际的输出电流是1.5A,这样会导致适配器过载发热,ICO可以优化这个问题,但是我打开了好像没成功。我是这个做的:

ico:
1. 使能EN_ICO_MODE
ChargeOption3 Register (SMBus address = 32h) Field Descriptions
[11] EN_ICO_MODE
2.
wait 2s ChargerStatus Register [14] ICO_DONE

3. IIN_DPM Register 22h [8-15] read
    copy 22h to 3fh
4. IIN_HOST Register 3fh

一直停在第二部,也就是ICO_DONE 不为1.

请问要怎么解决?谢谢。