如上图,输入设计电压DC12~24V,焊接多块电路板,电路工作正常,但LM3485芯片都烫手,其它芯片工作正常,当取下CA3电容时,17V以上输入电压时,LM3485就正常了,只要输入电压低于17V,LM3485芯片立即烫手,不知道为什么,是否有谁碰到过这个问题,帮助分析分析,是什么的问题?
我的几个电路都采用上面的电压设计,都莫名其妙的出现LM3485芯片烫手,调试了好久,有的电路只要去掉CA3,把RD1和RD2换成另一种相同比例的阻值就好了。有的就一直存在烫手的问题。PMOS采用的AO4411,Qg也是非常小的啊,也采用过AO4421,也是一样的问题