This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25700充电问题



您好,我们方案中选用的电源适配器是12V的,电池用三节电池串联,电池串联之后的最大电压在12.6V作用,

在这种情况下,12V的电源适配器通过BQ25700给电池组充电,充电电压可以高于12V吗?是否需要电源适配器电压

大于电池组电压,电池才会充电?

  • BQ25700是可以自主实现无缝升降压的,DC电源直接提供12V恒压给25700就行,充电电压到底是多少一般是锂电池上有电量监测计自主根据电池情况发送给25700的,打个比方你电池充满的情况下是12.6V,你这边如果没有数值,可以自行通过写寄存器来控制25700的充电电压和电流,你写的这个电压值如果比12.6V大,25700芯片内部电路可以做升压处理,虽然你恒压源只提供了12V,但是25700的输出可以提供更大的充电电压,看你自己的设定。
  • Hi
    这款芯片是升降压topy, 输入电压及可以高于电压,也可以低于电池电压。