This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895具体支持哪些快充协议

Other Parts Discussed in Thread: BQ25895

1、BQ25895具体支持哪些快充协议?

2、输入电流是怎么限定的?

3、关断电流能达到多少?浪涌电压,ESD等级如何。

  • Hi
    支持 USB2.0、USB3.0 标准
    Input current limit Input. ILIM pin sets the maximum input current and can be used to monitor input current
    ILIM pin sets the maximum input current limit by regulating the ILIM voltage at 0.8 V. A resistor is connected
    from ILIM pin to ground to set the maximum limit as IINMAX = KILIM/RILIM .
    关断电流,浪涌电压和你参数设置有关。