This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCDC输出电压精度的问题



DCDC数据手册上标准的精度跟什么有关系?有些标的是1%,有些标的是2%,我想问这些精度是由什么差异造成的?固定输出电压的是跟芯片内部FB的分压电阻精度有关吗?那可调输出电压的DCDC精度跟什么有关呢?另外VFB的电压也有个MIN和MAX值,这个精度会影响DCDC输出的电压精度吗?谢谢!

另外DCDC是不是没有PSRR这个参数啊?

  • Hi
    DC/DC输出精度,主要是由FB精度和FB反馈电阻的精度决定,VFB精度一般在1%左右(具体看芯片datasheet), 电阻也一般选择1%精度的,总体输出精度一般是在2%以内(不是叠加,但是一般规格都不会很偏,所以分布一般都是在2%以内)
    PSRR是针对LDO的,DC/DC里没有提这个。