Hi
目前在选型阶段,我想了解下LMR14030是否可以通过PWM占空比调整来控制输出电压,输入电压24V,输出电压0V-24V,步进0.01V,精度±0.01V
PWM由MCU产品固定频率脉冲,通过调整占空比来控制输出电压,另外对于FB端控制部分是否有参考电路,麻烦指教,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Johnsin
我在请教别人时他有提过使用TPS5420时有提出以下内容:不过TI芯片有种软启动方式不知你听过没,上电时软启动引脚向软启动电容充电,当电容电压低于基准电压时,FB电压等于软启动引脚电容两端电压,当软启动电容两端电压大于基准电压时,FB电压为基准电压。我曾经尝试过控制软启动引脚电压来控制输出电压,挺好用的,不知以上的说明是否可以实际实现,以及如何实现,需要什么样的硬件和软件支持,谢谢!
Hi Johnsin
另外补充问题,关于你说的:用TPS54308这类模拟芯片做会简单,因为不需要编程。你可以通过将PWM滤波成为直流,或者直接MCU的DAC输出。需要高精度,或可以通过MCU侦察,再调整,这样一个闭环的控制。通过PWM滤波为直流或DAC输出是直接接到FB端吗,FB是否还需要接下拉电阻或上拉电阻?MCU检测是直接检测输出电压还是检测PWM滤波的直接或DAC输出的电压,还麻烦详细说明下,非常感谢!