This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5025A 占空比突然变化的问题

Other Parts Discussed in Thread: LM5025A, LM5025

您好!

我们公司在使用LM5025A时出现以下问题:

 LM5025A芯片用于有源钳位正激控制,测试中出现以下问题:

 电路不装外壳测试,能够长时间稳定工作;

当装入金属外壳,同时有其他电路工作情况下,电路拉重载, 输出PWM占空比突然由稳态的30%转化为80%;此时,芯片COMP和RAMP信号都正常;随后芯片CS2脚过流,触发了芯片保护并开启软启动,

波形图请参考附件。

绿色是COMP信号,反馈信号。

蓝色是输出PWM波形,(蓝色占空比突然增加到最大)

黄色是RAMP,斜波信号。(斜波信号正常,但是斜波信号在低状态下,PWM信号也应该被拉低,但是实际没有拉低,触发过流)

是否可以帮忙给出一些建议来解决该问题?另外,LM5025芯片ABCD版本到底有哪些区别,是不是A版本抗干扰最差呢???

感谢!