在<bq769x0-3节至15节串联电池监控系列.pdf>中的均衡部分有这样一段话:The total duty cycle devoted to balancing is approximately 70% per 250 ms. This is because a portion of
the 250 ms is allotted for normal cell voltage measurements via the ADC.那么意思是说每一节电池在其均衡时会有12.5ms的时间用于电池采样,那么在电池采样的时间里对应的电池均衡的FET是关闭了吗?那下一个250ms周期再判断是否需要均衡,需要的话再打开对应的FET,是这个意思吗?还是指在电池采样期间均衡的FET不会关闭,我真的不太理解;还有就是均衡电流,在表格里写的是对于BQ76930和BQ76940最大的ICB(cell balancing current(internal ,per cell))是5mA,对于BQ76920的最大ICB是50mA,那么我现在用的是BQ76940,内部均衡 ,那均衡的最大电流只有5mA是吗?这个电流是怎么计算的,内部均衡电阻是多大呢?谢谢!均衡部分真的效果不好,我想知道正确的均衡流程应该是怎么样的,应该怎么使用内部均衡电路