This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116外加LM358恒流工作时不稳定

Other Parts Discussed in Thread: LM358, LM5116, LM5117

输入24-70V,输出13.8V7A,用LM5116外加LM358恒流电路,频率150K,恒压工作时系统稳定,恒流时声音大,波形不稳定,下MOS驱动工作一会,停一段时间,频率几百HZ,所以声音很明显,调节358环路没有改变,不知有没有人碰到类似问题?

  • 亲;由于LM358构成的电流环内包含了高滤波常数的LC滤波;导致反馈信号严重滞后而变得不稳定。建议降电流反馈移到滤波电解前试试。
  • 大侠,怎么移动?能否画一下,指示出来。

  • 就是将取样电阻放到滤波电容前面,另外还有几个问题,一是电流信号本来就小直接参与反馈容易受干扰,最好放大后再参与反馈,第二个是反馈输出电阻用10欧姆太小了,输出很小的扰动都会导致较大输出变化,根据你的调整范围选择合适的电阻,你换个2K的看是不是会好很多
  • 采样电阻放到电容前面也试过了,反馈输出电阻也调过,电流反馈输出接到COM端也试过,都不行,电流信号放大没有试

  • 有没有其他成熟的方案,输入24-70V,输出13.8V7A恒压恒流的?
  • HI
    看看LM5117: www.ti.com.cn/.../lm5117.pdf (第33/34页)
    只是最高电压建议在65V.