This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL455A-Q1通信问题



大家好!请教一个问题:我自己画的2层板,外接的电源,大于20V。WAKEUP 端串接一个10K电阻,接一个电源:3.5V,做触发唤醒信号。触发后,将电源降到0V。2个电源共地,用万用表测量 TOP NPNB VP VDIG VM V5VAO VREF 电压值均正常。我另做一个通信板,波特率达到1MHz,电源取至455A-Q1板。455A-Q1的RXD的上拉在455A-Q1板,TXD的上拉在通信板。通过串口调试助手,向455A-Q1板发送读芯片地址的命令,TXD端午反应,没有回码。用示波器在RXD端截取发送数据的波形,经过分析得到的数据和通过串口调试助手(波特率:250KHz)发送的数据一致。