This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电压我看了下都正常。现在发现很奇怪。我把输入电压加到19V时就可以充电。 但不稳定有时上电还是充不了,感觉是一直在休眠模式。电压在12V时就无法启动充电。
你好,
PG为高时VCC为无效值,请检查IC各个点电压值是否正常。STAT1与STAT2 均为OFF时:Charge suspend, timer fault, overvoltage, sleep mode, battery absent
另外,可以提供输入电压19V时的上电波型以及原理图吗?谢谢。
后续我提供上电波形。现在发现个现象,当电池电压低于8V时,12V是可以充电的,而且可以把电池充满,状态指示灯都正常。当电池电压高于8V以上后,断开12V电源再接上时就不能启动充电。
你好,
原理图中BTST电容C22推荐使用0.1uF;R29需要并联一个22pF电容;另外,请检查VCC电压以及BAT电压是否正常。
谢谢了,问题解决了,是C22电容值大了,换成0.1uf的就好了。谢谢!以后得多注意了。