This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A工作失调



您好!我是用3串锂电池包对设备的3串锂电池直接充电,输出电流3A。功能可以,但是有个问题,随着充电过程的进行,输出电压慢慢升高,输入电压慢慢降低,当输入输出电压比较靠近时,电感上的波形就会变比较杂乱,IC工作感觉有点失调,效率从97%下降到93%左右,因此MOS和25703A都会比较热。PCB已经参考设计打样几次,应该不是PCB布板问题,请问可能是什么原因? 软件上有可以设置的地方吗?

谢谢!