This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

用TPS51200+TLV62130搭建FPGA电源树方案咨询

Other Parts Discussed in Thread: TPS51200, TPS54620, TLV62130

上图为FPGA开发板设计的电源框图,通过Power good信号,按顺序级联,以1.0V->1.8V->1.35V->3.3V的顺序完成上电顺序。

下图是实际原理图:

图1:是两个芯片并联在一起,提供1V、6A的电源

图2:用图1的PG来控制1.8V的EN

图3:用图2的PG来控制其EN

图4:用图3的PG来控制其EN

图5:

问题:1.这样的电源树设计是否合理,级联起来会不会有什么问题

          2.LC参数是否需要修改

          3.  1.35V的电阻分压参数是否合理

          4.TPS51200直接用1.8V控制其EN端是否合理