您好,我的需求是用USB type c充电器(华为的 ,支持5V 2A 或 9V 2A)给设备充电(Type c 接头,电池为2S,充满8.8V),选用bq25703a是否可以?如何给bq25703a开启快充呢(用9V充电)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
对于charger IC来说,设置好电池电压以及充电电流即可以实现充电。至于Aapter的输出电压9V设置,可以参考上面的参考设计。
参考文档里,有一段描述是:该器件使用三个输入引脚(PSEL、HIPWR 和 PCTRL)来配置传输的电压和电流。该器件会根据接入接收器的电压请求,使用 CTL1、CTL2 和 CTL3 引脚选择所需的电源电压。问题是,我接收器是BQ25703a的话,BQ25703a会发出该电压请求吗?我在手册上没有看到类似的描述。
你好,
BQ25703a只做充电功能,不进行对Adapter的输出配置。这里需要另外的IC来进行快充的握手协议,如支持 BCDv1.2 的充电器检测器件bq24392或者是支持PD 协议的Tps65981等。