This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH05050WAH输入输出电容问题



PTH05050WAH的数据手册上说输入端可以采用2个47uF的陶瓷电容,“Total capacitance of 94 µF is acceptable based on the combined ripple current rating”,请问使用一个16V 100uF的陶瓷电容是否可以,请问陶瓷电容的ripple current怎么确定,另外低温条件下,PTH05050WAH的输入输出电容是不是采用钽电容和陶瓷电容的组合效果更好,钽电容和陶瓷电容的容值大概应选择多少呢?多谢!

  • 你好,用陶瓷电容也可以。耐压够的话100uF没问题。不需要组合,只用陶瓷也可以,陶瓷也有不同等级的,可以选温度特性好点的,不然电容容值变化太大,谢谢。
  • 你好,现在有一个问题是PTH05050WAH需要的5V电压有traco power的THL 3-2411WI 提供,看了一下THL 3-2411WI的最大Capacitive load是220uF,PTH05050WAH各需要100uF,还有另外一个LDO我接了20uF,但用LCR表测量总电容是280uF,PTH05050WAH芯片自己就有30uF左右的电容,请问这种情况可以正常工作吗,还是我需要把THL 3-2411WI 换成Capacitive load更大的模块,比如TMR 9-2411WI,最大Capacitive load是1300uF,多谢!
  • Hi
    建议实际调试确认,主要电压是稳定的,可以适当减小电容。