你好,我使用TPS5450将12V降压到5V,输入电压是OK的,但输出电压一直都是在1.7V左右,反馈引脚的电压为7.6V(按理说应该是1.2V左右的),反馈电阻分别是10K和33K。续流二极管用了SS54,官方给的是B540,后来我用SS54尝试过是可以的。以前用这电路是没有问题的,请问是什么原因呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我使用TPS5450将12V降压到5V,输入电压是OK的,但输出电压一直都是在1.7V左右,反馈引脚的电压为7.6V(按理说应该是1.2V左右的),反馈电阻分别是10K和33K。续流二极管用了SS54,官方给的是B540,后来我用SS54尝试过是可以的。以前用这电路是没有问题的,请问是什么原因呢?