This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5008MM输入92V烧毁,输入48V正常

Other Parts Discussed in Thread: LM5008

用LM5008做个小电流DCDC,12V输出,现在输入接48V,一切正常,输入如果接92V,芯片就烧毁了。

每次损坏的位置都一样,输入电压不是写的100V吗,为什么92V就烧了。

  • Hi
    推荐最大电压95V,超过100V烧的机会非常高。
    如果是稳定的92V是没有问题的。
    很可能是你输入不稳定,有电压上冲。
    也可能是你输入连有导线,输入走线不好,这样会导致寄生电感,芯片在启动时,因为寄生电感会产生振荡,很容易出现超过100V的电压。
    如果是这样,需要在导线接入端增加一个较大的电容如100uF以上。输入走线尽量宽一点,输入电容尽量靠近芯片输入端。
  • 您看下我的原理图有问题吗?只焊接芯片,其他元件不焊就不会烧,都焊上,电压高就烧了。这个是过压烧的还是过流呢,负载没接,现在就有个10uF电容,十分感谢
  • 加大电容就好用了,十分感谢
x 出现错误。请重试或与管理员联系。