参考TPS65131 EVM搭的电路,+5V输入,+-15V输出,前两天还正常,突然昨天开始发现+15V输出减半(-15V正常),FBP电压也变成了0.6V(FBN正常1.2V),Vref正常1.2V。
于是开始逐个更换外围元件和TPS65131,情况还是没有改观。
今天继续调这个电路,直到现在半夜,还是没有结果,故发帖求教经验,谢谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi :
是否有确认你的负载? 请在轻载下启动,看是否正常输出?
正常而言,TPS65131, 电流限制是1.8Amin, 如果负载过大,或者电感饱和都会导致输出电压异常(偏低的),请问您的电感饱和电流的规格是多少?(EVM板上的4.7uH电感是1.8A规格的)