This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LM1117IMPX-3.3/NOPB电源的一个问题



关于LM1117IMPX-3.3/NOPB电源,5V输入电压,3.3V输出,带载电流200mA左右,该芯片已使用3年;现出现故障,故障现象是输入电压5V输出电压为4.1V;LM1117IMPX-3.3/NOPB芯片焊接的单板整体做过三防,故障发生后,为了排查问题,重新更换新的LM1117IMPX-3.3/NOPB芯片,对设备进行过静电试验(直接接触放电增加到12KV,高于标准)、高压实验进行排查问题,未复现LM1117IMPX-3.3/NOPB芯片故障现象,现求助各位大神,帮忙分析分析,会不会是芯片失效导致,或者导致输出4.1V的现象还有什么其他的可能性原因。

  • Hi
    确认一下,首先是正常的,工作一段时间后(3年内),开始出现芯片不正常? 现象是3.3V输出变成了4.1V, 更换芯片后正常,然后怎么也复制不出这类不良? 不良率是多少?
    建议就单体分析,找一下授权代理商,将芯片开盖,可以看到是EOS还是ESD.
    倾向是前者,输入如果过压烧掉,可能导致输出异常,输出随机,不一定每次都是4.1V.