This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq78350 使用auto ship與sleep的選擇考量



目前應用在Chemistry中可選到相對應的電池型號,但因考量壽命問題,縮小使用範圍從2~4.25V變更為3~4V,

變成RSOC不準,但做過learning後變得比較準,因考量長途運輸選擇ship功能(自耗小),但ship等於shutdown,

再重新開啟,RSOC會從100%變成75%,大家都是選擇哪一種模式呢?

  • 你好,

    这种现象可能是使用电压范围选择不合适,RSOC是关于使用终止电压的一个函数。建议你不要将电压的最小值设置为3V,因为这样对电池的寿命影响不大,建议重新对该电压进行调整,比如将最小电压设置为2V,然后再观察RSOC是否还会从100%降到75%。