我设计了一版LED背光驱动电路,参照TPS61197EVM绘制的原理图,在常温下工作正常,一旦进入低温-30℃以下,基本上是10片有4 5片挂掉,-40℃基本上全挂,目前最有效的办法为更换芯片,无有效解决办法,所有器件均选择的-55℃~125℃的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我设计了一版LED背光驱动电路,参照TPS61197EVM绘制的原理图,在常温下工作正常,一旦进入低温-30℃以下,基本上是10片有4 5片挂掉,-40℃基本上全挂,目前最有效的办法为更换芯片,无有效解决办法,所有器件均选择的-55℃~125℃的。
芯片为一个批次,总共20片,目前经过试验后,仅仅2片能经得住-40℃。这2片更换到任何其余电路都不会有问题。目前已试验过多次,未出现故障。这是我公司第二次购买该芯片,第一批次20片有8片抗住了。按照原理芯片在满足启动的外部条件后,VDD会升压至7V,之后启动REF引脚端的恒流源输入200uA的电流至电容,给电容充电至2V,在这个过程中当Vref超过Vovp后触发BOOST过程。Vref无法升压所以无法触发BOOST过程,从芯片机制来说,应该Vref升压应该和外围电路关系不大,所以目前定位还是是芯片本身有问题。因为是第一次使用该芯片,所以很担心这个问题。
谢谢答疑!