This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请帮忙确认SLVA209文档中 TPS61040 180V at 4mA方案的稳定性和可行性,主要帮忙分析MOSFET导通时SW承受的电压和标称电压相关风险

Other Parts Discussed in Thread: TPS61040

请帮忙确认SLVA209文档中 TPS61040 180V at 4mA方案的稳定性和可行性,主要帮忙分析MOSFET导通时SW承受的电压和标称电压相关风险,谢谢

目前使用SLV209中的TPS61040 180V方案

一种分析,SW的承受电压是28V,但是MOSFET导通时,二极管阳极的一个脉冲电压直接导通到SW端,该脉冲电压的最大值达到179V左右。尽管DC很小,但是本人还是担心有一定的风险。

该电路的另一种分析,Q1导通,Q2 s端拉低,Q2导通,Imosfet为流过Q2 ds,Q1 ds,R1的电流。Vsw=Imosfet*(R1+Rq2dson),而Imosfet max=0.4A(OCP current),Rq2dson=1ohm,so Vsw=0.4A*(R1+1ohm)=0.4*R1+0.1V,这个值的大小取决于内部电阻Rsense 及如图R1。Rsense TPS61040和SLVA209中没有提到具体的值。Rsense 取值应该很小,所以Vsw会很小,大部分电压差在Q2 ds端。

以上两种分析第二种分析更科学。希望有更专业的人来确认该方案的稳定性和可行性,谢谢!