This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于降压型电源芯片LM5575的疑问

Other Parts Discussed in Thread: LM5575, LM5018, LM5165

你好,我们目前考虑使用LM5575作为我们的DCDC芯片,我们的需求如下:
输入电压:8V~65V
输出电压:5.3V
输出电流0~120mA。
目前有以下几点疑问:
1、在LM5575的datasheet中描述,要让其工作在连续传导模式,要保证流过电感的最大纹波电流小于2倍最小负载。然而我的电路板中可能某些情况下消耗的电流比较小,那这样是不是就没办法选电感了,如果LM5575工作在断续模式下会有什么问题?
2、LM5575的最大负载电流是1.5A,而我需要的电流最大是120mA。我们公司有电子负载,如果我们选用动态负载(半载-满载切换)去测试整个环路的稳定性的话,电子负载设置的吸入电流最大值即满载情况下是1.5A还是120mA?
谢谢。