This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS71718DCK电源芯片输出电压与的用户手册的应该输出电压不一致

Other Parts Discussed in Thread: TMS320C6748

1、TPS71718DCK芯片的用户手册显示输出电压应该是1.8V,我用该电源IC输出电压为什么是2.9V?

我买的这个芯片封装标签是BMX,查了一下,对应的就是TPS71718DCK;而TPS71729的封装标签是BMZ,所以可以排除购买型号错误的原因。

2、此外,我把该芯片的输出引脚翘起来,然后通电测它的输出,发现输出是1.9V左右,更说明型号正确,然后测翘起引脚对应焊盘的电压,结果是2.9V,我在想会不会是这个的影响? 

3、TPS71718DCK是为TMS320C6748芯片的DVDD供电,如果电压不对会不会对烧写程序有影响?

 有点着急,万望回复,不胜感激!

  • 1.TPS71729有 TPS71729DCKT的型号,封装与TPS71718DCK一样,请您再次确认您的型号。
    2. 关于您所说的“测翘起引脚对应焊盘的电压,结果是2.9V”能否具体说明?请您确认下的封装是否画正确,封装请参考datasheet第37~38页。
  • 感谢回复

    1、型号确认了,的确是TPS71718DCK。 您说得没错,TPS71729DCKT与TPS71718DCK的封装一样,都是SC70;但我上面所说的“封装标号”不是指元器件对应的封装,而是它们表面外观上的印刻字母,这个不是封装代码;是不是不同型号上面的刻印字母不一样?

    2、“测翘起引脚对应焊盘的电压是2.9V”。意思是TPS71718DCK有5个引脚,我把输出的那个引脚翘起来(即让此引脚离开焊盘,其余引脚依然焊在电路板上),然后测翘起引脚的输出,为1.9V左右,这应该可以证明芯片型号没错,TPS71718DCK的输出就是1.8V左右。然后引脚翘起来后,它对应的那个焊盘就空了,我就测焊盘电压,测出来值为2.9V。

    3、我的TPS71718DCK是为TMS320C6748芯片的DVDD18供电,如果电压不对会不会对烧写程序有影响?