This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电池快充type-c接口方案选型

Other Parts Discussed in Thread: BQ25895, TPS65981

TI工程师您好:

现在要做一个设备,自带单节锂电池2000mA时,设备内系统板工作电压5V,需电流2A max。设备仅有一个type-c接口,需要握手电源适配器端标准的PD 3.0协议。支持边充电边工作(电源路径管理),插拔适配器后级5V不会掉电。

请帮忙推荐一个IC,不需要支持双向快充,仅受电快充就好,能使得电池输出5V?

  • 使用TYPE-C接口,必须是快充IC支持type协议才可以是吗?还是说依然可以使用type-c接口内的D+ D-,来做和USB A 一样的识别?
  • 这两天看资料:
    我的需求就是:最好一颗IC ,完成与供电端的快充协议握手,并能将电池boost到5V输出给后级供电,并支持边充电边让后级工作,不需要快充输出。看BQ25895是可以的,但快充输出功能不需要用,太浪费了。有没有更合适的芯片。
    如果没有是不是,用两到3颗IC来完成,一个USB快充识别芯片如NT6008、一个电源路径管理芯片?
  • 你好,
    如果是要进行PD3.0握手协议,需要使用PD controller,可以参考TPS65981,可以搭配使用host-control类的充电芯片。