This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS73633可以并联使用吗?



想做电源之间无缝切换,涉及到两片TPS73633并联使用的情况,请问这款芯片可以并联使用吗?如果不能该怎么解决?万分感谢!!!

  • 两片TPS73633分别接不同电池组,只有输出端并联,这样可以正常使用吗??
  • 您好,想请教两片TPS73633输出端并联,可以正常使用吗?两片TPS73633的输入端分别接不同电池组;具体就是,一组电池容量小,一组容量大,系统待机状态下我用小容量电池组经过TPS73633稳压后供电,当有大容量电池组接入系统,最终经过另一片TPS73633稳压后,我再切断小容量电池组经过TPS73633稳压后的3.3V供电,期间会有两片TPS73633输出端并联的情况,不知道这样设计能否正常工作?
    另外,由于两个电池组电压幅度不一样,大容量电池组,需要先经过一片稳压芯片,然后才经过TPS73633稳压为3.3V,而小容量电池组,是直接经过TPS73633稳压为3.3V。
  • 并联的话建议在输出端各加一个二极管隔一下,否则会有一个存在反灌问题

  • HI
    在LDO的输入输出之间增加一个肖特基,当电压输出反灌时可以保护LDO.
    不建议在输出增加二极管,这样有压降,输出得到的最终电压就不是3.3V了。如果加载输入,电池效率降低。
    如果不嫌麻烦,选择Oring芯片或也可以,通过MOS替代二极管,例如LM5050.