Other Parts Discussed in Thread: UCD9222, UCD9244
尊敬的TI工程师们:
小弟使用UCD9222+7242对C6678进行CVDD的供电,之前配置输出正常。 但是做低温试验输出到不了1V,目前还没有查出什么问题。
现已更换芯片,设置还是跟之前一样,已取下DSP,无负载,却发现电压始终起不来。经测量 PWM信号是百分之九十多,没有fault信号。各路大佬能否给小弟一些提示,或提供具体的参数信息帮忙分析,感激不尽!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
非常感谢您的回复,上图为原理图和监测图。
调试内容主要有:
输入为5V,输出1V。检查9244到7242的外围电路及反馈电路发现没问题。
以上是在没开启TON_MAX的时间限制,状态寄存器只有POWERGOOD为黄色。