在做一个电池供电的设备,使用TPS63001将电池的3.6V变成3.3V,向MCU供电。
测试时,发现在空载的时候,输入电流大于5mA,看到手册上写的时小于50uA,请问测试的结果正常么?
原理图和LayOut参考的是数据手册的,外围器件值也一样,功率电感采用的时村田的LQH3NPN2R2NG0L 。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在做一个电池供电的设备,使用TPS63001将电池的3.6V变成3.3V,向MCU供电。
测试时,发现在空载的时候,输入电流大于5mA,看到手册上写的时小于50uA,请问测试的结果正常么?
原理图和LayOut参考的是数据手册的,外围器件值也一样,功率电感采用的时村田的LQH3NPN2R2NG0L 。
先确定电路中时候有其他耗电电路存在, 将EN拉低,看Iin电流有多少,如果有mA级别的,那应该就是芯片有问题,
同时在芯片空载工作时,检查L2端口的波形时候正常
电感应该是可以用的
L2的波形就是普通BUCK电路SW节点的波形啊,出来应该是方波,你传上来看看
powerpad要焊接上的,但是5mA的静态电流有点太大了,是异常情况
正常静态电流,空载时应该是小于50uA
看了你的原理图,基本没啥问题,输入电容有点多(但并不是问题),不过你可以尝试只放一个10uF的瓷片电容看下
排除下是不是存在电容漏电的情况,
测量了一下PS引脚。经过测试,50uA电流是在开启POWER-SAVE模式下测得的数据,而在关闭POWER-SAVE模式时,静态电流为5mA。这两个的值差别还是太大了。