Other Parts Discussed in Thread: LM5036, LM25119, LM5145
Dear,
有一个非隔离的DCDC项目,输入为:18~36V,输出为15V/45A。拓扑选择应该是单相同步整流BUCK或者两相交错并联同步整流BUCK,从热考虑,个人认为应该是选择两相交错并联BUCK比较适合。不知是使用2个独立的IC或者单个含2相交错功能的IC,哪个更好?帮忙推荐下IC或者解决方案。
另外,关于BUCK的芯片中定义的Iout(max),是否要求电路的最大电流要小于此Iout(max)值。比如我们要求输出45A,只能使用IC定义的Iout(max)要大于45A的?个人理解,由于MOSFET是外加的,那么IC仅作为控制,是否是Mosfet的驱动损耗导致对IC的Iout(max)要求?如果我们外加驱动线路来驱动Mosfet,则对IC的Iout(max)就没有要求了?
帮忙推荐针对此应用的IC,非常感谢!