This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI BQ76930的AFE 7个Cell connection问题

Other Parts Discussed in Thread: BQ76930

我是用TI BQ76930的AFE
如果是10个cell的设定, 相邻的cell 不能同时做Cell Balance
如CELL3和CELL4不能同时做Cell Balance

Cell Connections for bq76930 (10 cells)
CELL 1
CELL 2
CELL 3
CELL 4
CELL 5
CELL 6
CELL 7
CELL 8
CELL 9
CELL 10

但如果是7个cell 的connection, CELL3和CELL4之间有一个short
请问一下这时候的CELL3和CELL4算是相邻吗? 我可以对CELL3, CELL4做cell balance吗?

Cell Connections for bq76930 (7 Cells)
CELL 1
CELL 2
CELL 3
short
CELL 4
CELL 5
CELL 6
short
short
CELL 7


Thanks

  • Matt,

    算是相邻,还是不建议同时做CB。不建议相邻CELL同时CB,主要是从器件引脚绝对耐压和差分耐压考虑。可以参考下面文档的9.5章节

    www.ti.com/.../sluub41.pdf

  • If cells 4 and 5 are balanced, the VC3 input pulls to VC4, which is approximately the cell 4 voltage or 16 V.
    ==>请问一下这时候VC3,VC4,VC5的电压值各为何? VC3,VC4,VC5这时是等电压吗?

    However, if cell 1 and cell 2 are balanced, VC0 pulls to the cell 1 value of 4 V. Because this is above the absolute maximum of 3.6 V
    ==>是指VSS-VC0不能超过3.6V,如果每个cell是4V的情况下,是不是只要cell1做电池平衡时,VSS-VC0就会超过3.6V?


    Datasheet中的6.1 Absolute Maximum Ratings及6.3 Recommended Operating Conditions
    提到的电压值有什么不同,关于VSS-VC0,一个是3.6V,一个是写10V
    VSS-VC0的绝对最大额定值是3.6V
    (VC0–VSS): 10V

    这部分不是很了解
    不知道是否可以帮忙解惑一下


    Thanks