This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
tps7a8101的负载调整率我看了在0--100ma比较好,只有25mv左右,当然它最大电流是1a,但是我只用到100ma以下。 但是负极性ldo里边负载调整率都不好,比如tps7a30,100ma时达到200多mv。
HI
选择TPS7A33, 不过这些都是1A的LDO, 在500mA的负载动态变化时输出电压波动在50mV左右,所以100mA相信会小很多。
如果选择200mA左右的LDO,可考虑将输出电容适当加大,或者在反馈高边电阻上增加100pF电容并连,或都可以降低负载变化率。