This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27541-G1 I2C读数不正常



各位好:

        我们在使用BQ27541-G1读取电池电压、温度等数据时发现读数一直不正常,I2C接口我们是用普通IO模拟的,在和其他设备通讯时都正常,也都加了10K的上拉。在执行Module_bq27541_G1_ReadBatteryPercent时,读不到数据,DEBUG发现,程序在运行到Module_I2C_Software_ReadBytes_1时,在“//发器件地址+1(read)”时,无法收到ACK从而报错退出了。(如果无视此错误,继续读数,则会读到0x7FFF同样,读温度、电压时,也会出现同样的错误。请问这可能是哪里出现了问题?这部分的程序如下:

I2C_ErrorTypeDef Module_I2C_Software_ReadBytes_1(uint8_t ucIndex,uint8_t ucIcAddr,uint8_t ucRegAddr,
                                                 uint8_t *pucData, uint32_t ulNum)

        uint16_t  n = 0;
        I2C_ErrorTypeDef    ucError = I2C_ERR_OK;   

        //入口参数检查
        if (ucIndex > 4)                                                 { return I2C_ERR_PARAM_INDEX; } 

        //发送起始位
        ucError = I2C_SwStart(ucIndex);
        if (ucError) { I2C_SwStop(ucIndex); return I2C_ERR_SEND_START; }

        //发器件地址+0(write)
        ucError = I2C_SwSendSlaveAddress(ucIndex,ucIcAddr, 0);
        if (ucError) { I2C_SwStop(ucIndex); return I2C_ERR_SEND_SLAVE_ADDR; }
        
        //发寄存器地址
        ucError = I2C_SwSendByte(ucIndex,ucRegAddr);
        if (ucError) { I2C_SwStop(ucIndex); return I2C_ERR_SEND_DATA_ADDR; }
        
        //发送起始位
        ucError = I2C_SwStart(ucIndex);
        if (ucError) { I2C_SwStop(ucIndex); return I2C_ERR_SEND_START; }

        //发器件地址+1(read)
        ucError = I2C_SwSendSlaveAddress(ucIndex,ucIcAddr, 1);
        if (ucError) { I2C_SwStop(ucIndex); return I2C_ERR_SEND_SLAVE_ADDR; }

        
        //读ulNum个数据
        for (n=0; n<ulNum; n++)
        {
                if (n >= ulNum-1)   //产生NoACK
                {
                        ucError = I2C_SwReceiveByte(ucIndex,pucData, 0);
                        if (ucError) { I2C_SwStop(ucIndex); return I2C_ERR_RECEIVE_DATA; }                  
                }
                else                //产生ACK
                {
                        ucError = I2C_SwReceiveByte(ucIndex,pucData, 1);
                        if (ucError) { I2C_SwStop(ucIndex); return I2C_ERR_RECEIVE_COMPLETE; }                 
                }
                
                pucData++;
        }

        //发停止位
        I2C_SwStop(ucIndex);

        return I2C_ERR_OK;
}