你好,请问 TPS61088升压一段时间(几分钟或几个小时候)后停止升压,重新上电也不升压,放置几个小时后再上电又可以升压,是什么原因啊?
我用的是将3.7V锂电池升压到9V/1A.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,请问 TPS61088升压一段时间(几分钟或几个小时候)后停止升压,重新上电也不升压,放置几个小时后再上电又可以升压,是什么原因啊?
我用的是将3.7V锂电池升压到9V/1A.
看到一次实际情况是:正常工作VOUT为9.4V,突然不工作的时候电压会在7.5V--10.5V跳动5-6秒,然后慢慢下降到4.4V,停止十几秒,最后降到3.3V,然后一直就不升压了,重新上电也不升压,断电放置20几分钟再上电又工作正常了.