This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS59124使用的问题!

Other Parts Discussed in Thread: TPS59124

用TPS59124设计一款双路输出电源,输入电压4.5V~20V,输出可调,输出负载8A,按PDF典型应用画板,现在碰到以下2个问题。

1、在5V输入时,输出电压3.3V与1.2V,最大能带载的电流只能到4A,加大负载就无输出,也不能启动。

2、输入电压只能在6V以内,往上就就算是空载也无输出。