This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电源网络残余电压问题--是否是正常现象,如何定位?



各位好,最近在调试的时候碰到的问题:我的主板上有多种电压,包括12V 5V 3.3V 1.8V 1.0V,在调试的时候发现,当3.3V输入断开时,其他电压都是正常的,3.3V网络中依旧有电压,电压值大约为1.86V,请问1.86的电压是从哪里来的?是否会对产品的性能有影响?如何定位?

  • 个人觉得应该从两个方面进行分析

    1.你的这路电压是否是隔离的,如果不是隔离的,有可能是该路的等效电路跟别的电源分压呈现的这个电压.

    2.如果电源是隔离的,可能是干扰信号,你在3.3V输入两端接一个1K左右的电阻看看电压变成了多少,如果降低到几乎为零就是干扰造成的.

  • To weiwang1:

    理论上应该是隔离的,但是实际中板子上很多芯片都同时用到3.3V,1.8,或者其他两种甚至三种电压;芯片内部就不清楚了;

    我实验下你提到的第二点看看实验结果.....

    谢谢