This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24040 TS温度点问题

Other Parts Discussed in Thread: BQ24040

现在在用BQ24040做一款产品,NTC电阻按照规格书使用了10K(25°)

样品做测试在4°到53°还可以工作。低于4°或高于53就停止工作了。

现在客户有要求要在0°到55°都能正常工作,我想请问有什么办法可以做到,还有资料显示这芯片是不是不可以在O°使用。