我们在之前的产品设计中使用TPS73633DBVRG4(丝印T46),用作5V转3.3V电源,一直很稳定。
但是在最近设计的一款新的产品中使用的是TPS73633MDBVREPG4(丝印T64)芯片,属于TPS73633-EP系列,同样用作5V转3.3V电源,电路设计同原来的设计相同。打样生产的两张电路板,在芯片输出端均输出5V电压,无法输出3.3V电压。经过测试后发现输出跟随输入,无法实现降压。在这之后陆续测试剩余的TPS73633MDBVREPG4芯片,发现全部都是这样的情况:无法实现降压。最后一颗芯片,我们没有焊接在电路板上,直接对引脚供电,没有使用电容滤波,也是同样的情况:无法实现降压。
请问这两款芯片(TPS73633,TPS73633-EP)有使用的差别么?我在手册中看到的电路,二者一样的。