This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCP020505U输出异常问题



ALL:

          我们在用DCP020505U的时候发现,当我5V输入,输出加不同的负载则输出电压不同,具体如下:空载的时候 输出8.0V,3K负载的时候 输出6.1V,1K负载的时候  输出5.7V,36欧姆负载的时候  输出5.1V。手册中有如下图,是不是意味着这颗芯片在不同的负载下是会有不同的输出电压?但是从图中看DCP020505U在空载的时候也不会超过5.7V才对,难道必须要在输出功率达到2W的时候才能稳定在5V吗?如果负载不是12.5欧姆就不能使用这颗隔离电源?